Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the standard amps per square inch on panelboard bussing?

Article available in these languages: Spanish

Issue:
How is the standard amps on panelboard bussing rated, per square inch , temperature?

Product Line:
Circuit breaker panelboards sold and supported in the USA.

Environment:
Application

Cause:
Specification

Resolution:
Manufacturers have a choice of testing their panels by amps per sq. inch or heat rise.
Schneider chooses to test by the heat rise method as we feel it is a better test of how connections and joints will react based on actual temperatures rather than the sq. in. calculation method.

We don't have an amps per sq. in. rating for our panels. If per square in rating is needed, it would require the selection to High Density Buss option of 750 amps per sq. in. for Aluminum, or 1000 amps per sq. in. for Copper in product selectors.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings