How can we help you today?

What are the dimensions of the EVlink pedestal base?

Issue:
Layout of the pedestal base for mounting

Product Line:
PTEVC - Electric Vehicles

Resolution:
The Pedestal base dimensions (metric) are shown below and are also available in the Installation Manual for Outdoor EVlink stations. Base dimensions are the same
for all Level 2 pedestal offers. Anchor bolts of 12.5mm (1/2") will easily fit the provided slotted openings, and a 50mm (2") stub will fit the central opening.
Pedestal Base Dimensions

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors