Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the EX Transformers available in Nema 4X Stainless Steel enclosures?
Issue:
Is NEMA 4X Stainless Steel Enclosures available for EX Transformers?

Product Line:
LV Transformers

Environment:
Applies to the new EX transformers by SquareD/Schneider Electric

Cause:
Availability of Stainless Steel enclosures

Resolution:
No, the Nema 4X are all Sealed Resin Epoxy Encapsulated Transformers which are exempt from the Energy Act and have never had to meet the DOE efficiency requirements.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings