Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is included in catalog number VCP1032?
Issue:
Product Design features

Product Line:
Canadian Homeline Load Centers

Resolution:
The Catalog number VCP1032 is a Canadian Homeline load center value pack that inlcudes the below products:

1) Load Center catalog number CHOM1632M100GC (100 A, main breaker, 16 spaces, 32 circuits, indoor)
2) Quantity of 5 catalog number CHOMT1515 (1 pole, 15 A tandem branch breaker)
3) Quantity of 1 catalog number CHOM215 (2 pole, 15 A branch breaker)
4) Quantity of 1 catalog number CHOM230 (2 pole, 30 A branch breaker)
5) Quantity of 1 catalog number CHOM240 (2 pole, 40 A branch breaker)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings