Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
To turn ON and OFF a Powerpact H, J, or L breaker with a motor operator, can the control signal be either an impulse type or a continuous type?
Issue:
What kind of signal is needed to turn ON and OFF an H, J or L-frame breaker?

Product Line:
Circuit Breakers

Resolution:
For a Powerpact H, J or L circuit breaker with a motor operator in the automatic mode, the breaker can be turned ON and OFF by using either an impulse control signal, or a continuous control signal.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings