Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Extending a Float Rod (for 9036 and 9038A switches only)
Issue:
What parts are needed to extend a float rod?

Product Line:
Float Switches - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
To extend the length of a standard rod kit (for 9036 and 9038A switches only), simply add additional rod lengths:
9049T1 - 2.5' section Brass Rod
9049T1A - 2.5' section Aluminum Rod
9049T1S - 2.5' section Stainless Steel Rod
These rods are threaded and will screw into the existing rod; no additional hardware is needed.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings