Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can a BCM module programmed for 2w Modbus be used on a 4w Modbus communication system?
Issue:
Applying BCM programmed for 2 wire modbus to a 4 wire modbus system

Product Line:
Powerpact P/R and Masterpact NT/NW breakers with modbus communications

Resolution:
  1. With a newer Micrologic P or H trip unit, you may reprogram the BCM module to 4w.  This requires Micrologic trip unit firmware version 2010AK or newer.
  2. If the trip unit does not have this option or if it is an A trip unit, you may use a 2w to 4w converter, like CNV-100. See the attached instruction bulletin for more details.
  3. Schneider sales offices can also order a BCM programmed for 4w Modbus. Order the module number, 33106, in Q2C with a note that you want it programmed for 4w Modbus.
    BCM 33106 profile is available only on Q2C Tool. Contact regional field offices to support order submission for customers who are unable to access Q2C.

Schneider Electric Canada

Attachment(s)
CNV-100.pdf [167.91 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings