Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CHU366AWK, Series E5 (or E05) heavy duty safety switch?
Issue:
Previous Design Repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line-Load base assembly - 4055218650 (3 required; arc suppressor assembly not included)
Arc suppressor assembly - 4051270850 (3 required)
Lug assembly - 4405044601 (4 required per base assembly)
Line base phase insulator - 4055219301 (2 required)
Line-Load base mounting screws - 4020600901 (3 required per base assembly)
Handle assembly - 4051217251
Handle assembly mounting screw and washer - 2140122242 (screw; 2 required) and 2370100220 (washer; 2 required)
Door thumb retainer - 4405043301
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Cross Bar Insulator - 4055217801 (1 required)
Cross Bar Insulators - 4055217701 (2 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings