Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to remove contacts from a Harmony 22mm XB4/XB5 push button?
Product Line:
Harmony XB4/XB5 ZB4/ZB5 22mm operators

Resolution:
Using a small, flathead screwdriver lift up on the metal hooks that are attached to the back of the mounting collar. Pull the contact out of the base while holding the top of the block making sure that the black securing piece slides out with little resistance.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings