Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to Mount Contact Blocks to a Harmony XB4/XB5 22mm Operator
Issue:
How are contact blocks mounted into the operator in 22mm push buttons?

Product Line:
Push Buttons and Operator Interface

Environment:
XB4/ZB4 and XB5/ZB5 22mm Operator Push Buttons

Resolution:
Make sure you don't have power to any component during the installation.

1. Attach any contact blocks/lighting module by inserting the bottom plastic nub
2. Then press the contact until the metal hooks attach to the back of the collar.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings