Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION 8650 C - How Many Simultaneous Communications Ports Can Be Used?

Issue
Limitation on number of enabled physical ports to the meter will result in communication failure on the disabled ports.

Product Line
ION8650 option C

Environment
Communication Ports

Resolution
The ION 8650 C only allows three physical ports to be enabled at any given time, of which one is always the front optical port.

The meter has the capability to have up to six communication options (ports):

1) COM1: RS232 / RS485
2) COM2: internal modem
3) COM3: front optical
4) COM4: RS485
5) Ethernet
6) Cellular modem


Only two ports can be enabled besides the front panel optical port (Which is always enabled by default) .  In order to use other communication options, the enabled ports should be disabled first.  Otherwise this message will pop up:

ION Setup pop up message 'Maximum additional enabled ports: 2'


For information on how to enable/disable ports in an ION8650C meter, refer to FA284369 article.
For information on the maximum simultaneous connections that can be communicate on each port, refer to FA212335 article.
For documentation on the ION8650 meter, refer to the product page here.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings