Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Enable or Disable Communication Ports in an ION8650C Meter

Issue
A total of 6 communication ports could be available depending on the communication options on the meter.  However, only 3 ports (one has to be the front optical port) can work concurrently.

Product Line
ION8650C

Environment
ION Setup

Cause
In order to switch between ports, the enabled ports have to be disabled before another port can be enabled.  This process is required in order not to exceed the maximum allowable of 3.

Resolution

1.  In ION Setup go to the Enabled Ports tab:

Setup Assistant

Select one of the ports that is to be disabled and click Edit; the following window opens.  Select which ports are to be enabled or disabled and click OK to accept the changes:

Set Enabled Ports



2.  In Designer the Factory Module has the setup registers to enable/disable the communication ports.  Select a port and click on Modify to change the setting:

ION Module Setup

In case the number of ports exceed the 3 allowed, the following message appears:

Error if over 3 ports enabled

In the above case the Factory Module went to offline state.  Edit the module to disable the port and save to put the module back in online state.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings