Issue:
What is the voltage code for 8501XUDO and 8501XDO industrial relays?
Product:
Industrial control relays, 8501X, 8501 type X, Type XDO, Type XUDO
Resolution:
What is the voltage code for 8501XUDO and 8501XDO industrial relays?
Product:
Industrial control relays, 8501X, 8501 type X, Type XDO, Type XUDO
Resolution:
| For XUDO ONLY | |
|---|---|
| DC Voltage | Code |
| 6 | V50 |
| 12 | V51 |
| 24 | V53 |
| 48 | V56 |
| 125 | V63 |
| 250 | V67 |
| For XDO ONLY | |
|---|---|
| DC Voltage | Code |
| 6 | V50 |
| 12 | V51 |
| 24 | V53 |
| 32 | V54 |
| 48 | V56 |
| 72 | V58 |
| 90 | V59 |
| 115/125 | V62 |
| 230/250 | V66 |