Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CH366, Series E5?
Issue:
Design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055270351 (3 required; arc suppressor assembly included)
Load base assembly - 4055270550 (3 required)
Arc suppressor assembly - 4051270850 (3 required)
Lug assembly - 4025113650 (2 required base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required base assembly)
Handle assembly - 4051217251
Handle mounting screws and washers - 2140122242 and 2370100220 (2 each required)
Door thumb retainer - 4405043301
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Dust Shield - 4055215701
Cross bar insulator - 4055217701
Cross bar insulator - 4052217801

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings