Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the length of the remote display cable provided with the PM8214 and PM8244 meter?
Issue
User is requesting the length of remote display cable that comes with PM8244 meter.

Product Line
PM8000 series meters

Environment
Remote display metering

Resolution
The PM8214 (complete part number METSEPM8214), is provided with a display cable 3 meters long.
The PM8244 (complete part number METSEPM8244), is provided with a display cable 3 meters long.

Other remote display parts that are available:
METSEPM89RD96 - Remote display with 3 meters length remote display cable
METSECAB10   - 10 meters Length remote display cable

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings