Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the different standard key options for 22mm operators?
Issue:
Do we have other key type aside from Ronis key 455?

Product Line:
22mm Operators- GIC Product
XB4/ZB4 and XB5/ZB5

Environment:
US Product

Cause:
Product Selection and need to know if there are separate part number for it.

Resolution:
The standard key for a 22mm operator is a Ronis 455.  To order an operator with a different key, append the following suffixes to the part number:

12 - Ronis key 421E
10 - Ronis key 458A
14 - Ronis key 520E
20 - Ronis key 3131A
D - Ronis key 8D1

Note that not every suffix is available for every operator - check pricing system for availability of specific parts

Separate part numbers:

Ronis key 421E - ZBG421E
Ronis key 458A - ZBG458A
Ronis key 520E - ZBG520E
Ronis key 3131A - ZBG3131A
Ronis key 8D1 - ZBD8D1

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings