Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use XB5R or XB4R wireless push buttons for an Emergency Stop?
Issue:
Can we use XB5R or XB4R for an ESTOP?

Product Line:
XB5R / XB4R

Environment:
Wireless Push Buttons / Operator Interfaces

Resolution:
This technology cannot be used for hoisting applications (“raise/lower”, “left/right”, etc. movements) or safety applications (emergency stop buttons etc.).
The Harmony XB4 and XB5 wired pushbutton range or the XAC pendant control station range
have to be used for these applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings