Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What wire sizes will fit into the QONK1, 2, 3, or 4 neutral bars?
Issue:
Size of wire accepted

Product Line:
QO Load centers

Resolution:
The QONK1, 2, 3, or 4 will accomodate wire sizes of #4 to #14 Cu, or #4 to #12 Al.
These neutral bars have a 90C rating.
Wire Size by Type and Torques
CU Wire RangeAL Wire RangeTorque (in-lbs)
#14 (2 wires)#12 (2 wires)20-35
#12 (2 wires)#10 (2 wires)20-35
#10 (2 wires)#10 (1 wire) &
#12 (1 wire) (Solid or Stranded)
20-35
#12 (1 wire) &
#14 (1 wire) (Solid or Stranded)*
20-35
#10 (1 wire) &
#14 (1 wire) (Solid or Stranded)*
20-35
#10 (1 wire) &
#12 (1 wire) (Solid or Stranded)*
20-35
#10-14 (1 wire)#10-12 (1 wire)20
#8 (1 wire)#8 (1 wire)25
#4-6 (1 wire)#4-6 (1 wire)35
*(Wire of same type )

Installation instructions are attached.
Load Centre box label has specific allowances.

Schneider Electric Canada

Attachment(s)
40281-836-01.pdf [317.13 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings