How to connect using MODBUS/TCP or MODBUS/USB to CO2 WAG?
The CO2WAG software only supports Modbus RTU protocol but you can use the Telepace Studio template program to connect using MODBUS/TCP or MODBUS/USB.
When the CO2WAG software is installed the default directory for the Telepace Studio template is located at C:\Program Files (x86)\Schneider Electric\CO2WAG\TelePACE Files.
Or see attached file.
When the CO2WAG software is installed the default directory for the Telepace Studio template is located at C:\Program Files (x86)\Schneider Electric\CO2WAG\TelePACE Files.
Or see attached file.
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.