Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the operating temperature rating for the MD3604X?
Issue:
MD3604X operating temperature

Product Line:
MD Motor Disconnect Switch—Non-Metallic NEMA Type 1, 3, 3R, 4, 4X, and 12 Enclosure

Environment:
UL508 Motor Disconnect Switches

Resolution:
Can be used in an ambient temperature of -20 to 50C

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings