Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CHU361DSWC, series F7 (may be shown as F07)?
Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The replacement parts for the CHU361DSWC, series F7 (F07) are as follows. No other parts are available.
-Line/Load Base Assembly - 4056609150 (1 required; arc suppressor not included)
-Line/Load Base Mounting Screws - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: mechanism coupling and cover interlock defeat coupling may also be needed)
-Mechanism Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets; 2 required)
-Lockplate Gasket - 4050322803 (2 required)
-Lockplate Mounting Screw - 2194900001 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541000046
-Receptacle Mounting Screws - 4510280101 (4 required)
-Ground Lug - 4025101652 (3 required)
-Ground Lug Mounting Screw - 4020513503 (2 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings