Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many simultaneous connections can be made using Link150 with ION Protocol?

Issue
How many concurrent connections can be made using Link150 gateway with ION Protocol?

Product Line
Link150 (EGX150)

Environment
Gateway ION Protocol Concurrent Connection Support

Resolution​
Only 1 TCP/IP ION master can be connected to Link150 at a time.

Note: Using Link150 as a Modbus TCP/IP gateway, the maximum number of connections supported is 32.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings