Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a TeSys T overload relay be installed on a type S starter in the field?
Issue:
Would like to retrofit a TeSys T into an existing starter

Product Line:
TeSys T Motor Management Controller

Environment:
Pre-Existing Type S Starter Installations

Resolution:
The NEMA type S starters with melting alloy, bimetal, or solid state overloads use a different backplate, as well as different bus, from the starters with TeSys T overloads.
The backplate and bus are not sold separetly.
As such the TeSys T cannot be retrofitted to an existing starter, a new starter with TeSys T overload installed from the factory will need to be ordered.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings