Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum size branch breaker that can be installed in an NF panel with a 600A or 800A panel?
Issue:
Largest branch breaker that can be installed in a 600A or 800A NF Panel

Product Line:
NF Panelboards

Environment:
Application

Cause:
Clarification of Largest amp size

Resolution:
The largest branch breaker that can be installed in the panel interior is a 3 pole, 125 amp EDB, EGB, or EJB breaker. The largest single pole breaker is 70 amp.
A factory installed sub-feed LA, LH or LC circuit breaker (400A max.) and one JD, JG, JJ or JL circuit breaker OR two sub-feed JD, JG, JJ or JL circuit breakers per 600A or 800A panelboard, if there is sufficient extra room in the enclosure.  There is not a kit available. Note: (JJ and LC sub-feed circuit breakers cannot be used together).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings