Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the flame rating or fire rating of circuit breakers?
Issue:
Do circuit breakers have a flame or fire rating? Can they be exposed to flames, and still used afterwards?

Product Line:
Circuit Breakers

Resolution:
Circuit breakers themselves do not have a specific flame rating or fire rating. They do, however, have a temperature range for storage and operation (carrying load). If a circuit breaker is exposed to flames, the temperature would be far above that of the storage or operating range, and the breaker should be replaced.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings