Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is current unbalance calculated on the DM6200?

Article available in these languages: Czech

Issue
The Current Unbalance formula is not detailed in the DM6200 User Manual.

Product Line
DM6200

Environment
Reading verification

Resolution

The current unbalance is calculated using the following equation:

I unbalance = (Max phase current - Min phase current) / Avg 3 phase current * 100

For example:

Ia = 100 A
Ib = 120 A
Ic = 150 A

Therefore, Max phase current = 150 A, Min phase current = 100 A, and Avg 3 phase current = (100 + 120 + 150) / 3 = 123.33 A.

I unbalance = (150 - 100) / 123.33 * 100 = 40.5 % unbalance

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings