How can we help you today?

What is the rear connection kit for the legacy FA/FH breakers?

Product Line:
Legacy FAL/FHL unit mount breakers

Resolution:
The studs may be bolted directly to the bus or lugs may be attached to the studs. NOT UL Listed.

(2) - FAS20 - Shorter studs with 2-1/4" overall length and 3/8" diameter with 16 threads/inch
(1) - FAS42 - Longer studs with 4-7/8" overall length and 3/8" diameter with 16 threads/inch

NOTE: Long and short studs must be alternated on adjacent poles to assure proper electrical clearance.