Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
​How do I clear the F0071 on a GT100 unit?
Issue:
Clearing the fault code 0071

Product Line:
GT100, GT250

Environment:
Installations that use a three phase GT unit

Cause:
The fault code F0071 appears but it does not clear after pressing F1 and power cycling the unit

Resolution:
ONLY QUALIFIED PERSONNEL WITH PROPER EQUIPMENT CAN WORK ON THIS UNIT FOR TROUBLESHOOTING
If the code does not clear after power cycling the unit and pressing F1, you need to open and lock out and tag out the external DC and AC breakers.  Once this has been done and you confirmed no live voltages on the DC and AC side of the unit, you can close the S1 switch by using an adjustable wrench or some other means to simulate a closure.  You can then check continuity across the auxiliary switch S2, which is attached to S1.  You can confirm continuity at the CCU board in connections P2-9 and P3-3

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings