Issue:
Do the GV3P and GV2 aux contacts come installed as standard?
Product Line:
GV Manual Starters and Protectors
Environment:
North American Products
Resolution:
These do not come with auxiliary contacts preinstalled, but we have instantaneous contacts as well as fault signaling and short circuit signaling contacts as listed in the table below.
$ - Cannot be used with GV2GH7 insulator
% - Mounting of a GVAE contact block or a GV2AK00 visible isolation block on a GV2P
* - The GVAD is always mounted next to the starter
Do the GV3P and GV2 aux contacts come installed as standard?
Product Line:
GV Manual Starters and Protectors
Environment:
North American Products
Resolution:
These do not come with auxiliary contacts preinstalled, but we have instantaneous contacts as well as fault signaling and short circuit signaling contacts as listed in the table below.
| Description | Mounting Location | Max. # of blocks | Contact Type | Cat # |
| Instantaneous Auxiliary contacts | Front ($%) | 1 | NO or NC | GVAE1 |
| NO + NC | GVAE11 | |||
| NO + NO | GVAE20 | |||
| Instantaneous Auxiliary contacts | Left hand side | 2 | NO + NC | GVAN11 |
| NO + NO | GVAN20 | |||
| Fault signaling + instantaneous auxiliary contacts | Left hand side (*) | 1 | NO (FAULT) + NO | GVAD1010 |
| NO (FAULT) + NC | GVAD1001 | |||
| NC (FAULT) + NO | GVAD0110 | |||
| NC (FAULT) + NC | GVAD0101 | |||
| Short circuit signaling contact | Left hand side | 1 | SPDT | GVAM11 |
$ - Cannot be used with GV2GH7 insulator
% - Mounting of a GVAE contact block or a GV2AK00 visible isolation block on a GV2P
* - The GVAD is always mounted next to the starter
Released for: Schneider Electric Canada