Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement modules for a FI8IMA12 or FI8IMA12C and FI8IMA16 or FI8IMA16C?
Product Line:
Surge Protective Devices (SPDs)

Environment:
Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
The replacement modules for A, B, or C phase in the FI8IMA12 or FI8IMA12C is MA8IMA12 (one module for each phase).
The replacement modules for A, B, or C phase in the FI8IMA16 or FI8IMA16C is MA8IMA16 (one module for each phase).

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings