How can we help you today?

How to pulse an "Ext pulse module" in ION Setup

Issue
A pulse is needed to be sent through an Ext Pulse Module using ION Setup.

Product Line
ION Meters

Environment
ION Setup

Resolution
1) Open meter in Advanced Setup Mode by holding CTRL key on your keyboard and click on the meter.
2) Navigate to Ext Pulse Modules and double click on the module that you want to send pulse through.
3) Click on the Output registers tab.
4) Hold SHIFT key on your keyboard and left click on "Trigger"
5) From the menu, click on "Trigger". that will send a pulse to that output.
Output registers

Schneider Electric Canada
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
  • Product Selectors