Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION Setup Disturbance Alarm Setpoints show a scale factor of x 1.0 on CM4000, CM3000, and PM800 series meters
Issue
When attempting to configure Disturbance Alarms for CM4000, CM3000 or PM800 series meters via ION Setup software, the scale factors for Setpoint Pickup and Dropout will always show x 1.0, however the voltage scale is set to a different value such as x 10.

View picture below which is the Voltage Scale value on a CM4000 meter being set to x 10:
ION Setup

Picture below shows the Setpoint scale as x 1.0:
ION Setup Alarms

Product Line
ION Setup any version prior to v3.0.17033.01
CM4000
CM3000
PM800

Environment
Onboard Alarms / Events configuration (Disturbance Alarm Setup only)
Sag or Swell Setpoint Scale

Cause
The scale factor is being applied correctly in ION Setup, it is only displaying it at a constant value of x 1.0 for all the Disturbance Alarms

Resolution
Download the latest version of ION setup software by clicking on the following article: FA212816

ION Setup version v3.0.17033.01 and higher will have this fix applied.

View picture below which shows the corrected scale value for Setpoint Pickup and Dropout:
ION Setup alarm config

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings