Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the control voltage and coil resistance for part number 8501KPDR12V63?
Issue:
Need to know the control voltage for the coil, as well as resistance, for an 8501 type K with V63 voltage code

Product Line:
8501 type K ice cube relays

Environment:
North American Products

Cause:
The V63 information is not included in the current 8501 type K catalog

Resolution:
The coil voltage is 125VDC and the coil resistance is 7300 ohm.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings