Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
COM'X 200/210/510 control power options and power consumption
Issue
Com'X power supply options and the power consumption for each of the options are needed

Product Line
Com'X 200 (EBX200)
Com'X 210 (EBX210)
Com'X 510 (EBX510)

Environment
Power supply

Resolution
  • 100-230 V AC  (±15 %) (This option is only available in Com’X 200)
    • ​Power consumption: 26 W max
  • 24 V DC (±10 %)
    • ​​Power consumption: 26 W max
  • PoE using Ethernet port 1 (ETH1)
    • ​​Power consumption: 15 W max

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings