Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is The Replacement Control Station Plate for the Old 9001D 22 MM Operators in a Model 5 Motor Control Center?
Issue:
What is the replacement control station plate for the old 9001D 22 MM operators in a Model 5 motor control center?

Product Line:
Obsolete Model 5 Motor Control Center, MCC

Environment:
Products sold in North America

Resolution:
Part number 80420-007-05 is the replacement control station plate but the latch is in a different position.   Also order the  latch pin retrofit kit part 8042089350.  The kit includes the template, instruction bulletin, new plate, latch pin and rivet.

Schneider Electric Canada

Attachment(s)
80438-821-01.pdf [23.97 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings