Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do QED 2 switchboards NEMA 1 or NEMA 3R rated come with a solid bottom?
Issue:
Do QED switchboards come with a solid bottom?

Product Line:
Switchboards

Environment:
QED, QED2

Cause:
Product features

Resolution:
All Switchboards regardless if N1 or N3R are shipped with the bottom open. Closure plates are available as an adder if you need them. These will need to be removed as part of the switchboard preparation for installation and the customer will need to make any holes in the plate necessary for conduit entering the bottom of the switchboard. After the holes are drilled reinstall the closing plates.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings