Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Power Monitoring Expert (PME) Disabling the Alarm Annunciator
Issue
User would like to disable the Alarm Annunciator from the web banner in EcoStruxure™ Power Monitoring Expert (PME)

Product
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Web Applications

Resolution

PME 9.0 and Greater

1) In a web browser, navigate to the Web Applications by typing in http://[server name or IP address]/web into the address bar
2) Navigate to the Settings tab
3) Click on Alarms -> Alarm Views
4) The annunciator can be entirely disabled by setting underneath the "Annunciator" section to disabled or by deselecting alarms based on priority in the "Priority Classification" tab as shown below
5) Press Save

Alarm Annunciator 2023

PME 8.0

1) In Internet Explorer, navigate to the Web Applications by typing in http://[server name or Ip address]/web into the address bar
2) Navigate to the Alarms application tab
3) Click on "Settings"

Alarm Annunciator 8.1

4) Navigate to the Alarms tab and uncheck the "Show the Alarm Annunciator". Press OK

Alarm Annunciator 9.0

5) Close then reopen Internet Explorer to verify the changes took effect

PME 8.1 and PME 8.2

1) In Internet Explorer, navigate to the Web Applications by typing in http://[server name or Ip address]/web into the address bar
2) Navigate to the Alarms application tab
3) In the top right corner of the Alarms application, click on "Edit Settings"

Alarm Annunciator 8.2

4) Uncheck "Show the Alarm Annunciator" and press OK

Alarm Annunciator

5) Close then reopen Internet Explorer to verify the changes took effect

Here is a video with instructions on how to disable the Alarm Annunciator in PME 8.2:



If you would like to deactivate alarms please see: https://www.se.com/us/en/faqs/FA313760/ ,

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings