Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to determine the firmware version for Micrologic A, P and H trip units
Issue:
What is the firmware version for
  • Micrologic 3.0A, 5.0A and 6.0A trip units
  • Micrologic 5.0P and 6.0P trip units
  • Micrologic 5.0H and 6.0H trip units

Product Line:
Circuit Breakers

Resolution:
Micrologic A Trip Units (3.0A, 5.0A, 6.0A)
The Micrologic A trip units do not have a means to access the firmware version in the field. Since January 2010, they have been using firmware version V01.029.

Micrologic P and H Trip Units (5.0P, 6.0P, 5.0H, 6.0H)
The Micrologic P and H trip units have a means to access the firmware version in the field.
The trip unit screen must have a display (must be powered).
1. On the screen on front of the P and H trip unit, press the "wrench" button
2. Scroll down to "Micrologic setup", and press enter
3. Scroll down to "Breaker selection", and press enter
4. At the very bottom of the P or H trip unit screen is the firmware version (example: PLogic-2014AN)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings