How can we help you today?

COM'X510 is not logging or publishing data

Issue
After an unexpected meter reset, the COM'X 510 may stop logging data and publishing data, even after resetting or reconfiguring

Product Line
COM'X510

Cause
An unexpected power outage to the COM'X510.

Resolution
There is currently no solution. This issue may be seen in firmware versions  3.5.24 and earlier.
Latest firmware can be found here https://www.se.com/nz/en/download/document/ComX_510_v6.8.7/