Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do our internally mounted SPDs all come with a disconnect?

Issue:
Do Surgelogic internally mounted SPDs come with a disconnect?

Product Line:
Surgelogic Surge Protection Devices

Environment:
Internally mounted surge protectors

Cause:
An integral disconnect is needed for the internally mounted surge protection device.

Resolution:
All I-Line, Switchboard, MCC, QMB, and Switchgear internally mounted SPDs come with a disconnect. NF & NQ panels have an option in product selector to add a disconnect but the internally mounted SPD can also be direct bus connected.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings