Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ENVT wire be replaced? Can it be bought separately?
Issue:
Some trip units that measure voltage have a white wire labeled ENVT. This wire needs to be replaced.

Product Line:
Molded Case Circuit Breakers

Resolution:
The ENVT wire cannot be purchased separately and it cannot be replaced. Even though it may appear to be plugged into the trip unit, it actually is not plugged in, and trying to remove it will damage the trip unit. So if an ENVT wire is damaged or has been pulled out of the trip unit, the trip unit will need to be replaced.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings