Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Impulse or Latching Relay
Issue:
Is there a small latching or impulse relay that is offered?

Product Line:
Relays and Timers

Environment:
Modular Timing Relay

Cause:
Product Selection

Resolution:
While not a true latching or impulse relay, there is a timing relay which can be used in a similar function to one.  The RE17RMXMU is a continuously powered timing relay which will open/close its output contacts upon receiving sequential trigger signals.  In other words, one close on the trigger contact will change the output contact over for an indefinite time and another close on the trigger contact will change the output contact back.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings