Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How does the PK5RK retaining kit install into the proper QO, single phase, 150-225 A max, convertible mains load centers?
Issue:
Product Design Features

Product Line:
QO Load Centers

Resolution:
The PK5RK retaining kit secures one 2-pole (Requires 4-spaces) 150-200amp High Amp Branch Circuit Breaker to the Right side of the interior when used as a Back-Fed Main Breaker.
This retaining kit can ONLY be used for QO, 1-phase ONLY, 150-225amp, Convertible mains, Series S__ load centers.
The retaining bracket will mount over the face of the back-fed branch breaker and get secured using the single interior mounting screw included with the kit.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.
Danger label pic
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Make sure to obtain the correct 2-pole, QO 150-200amp branch breaker to be used as the back-fed Main Breaker and DO NOT exceed the maximum rating marked on each load center.
3) As shown in step 2, on page 2 of the intructions, remove and discard the interior mounting screw A from the base at the location shown in Figure 1.
4) Install the appropriate QO back-fed branch breaker ONLY in positions 2,4,6 and 8 (The first 4 positions in the upper right side of the interior). Also, see the instructions that come with the Branch Breaker.
5) Center the hold-down bracket (figure 1) over the branch breaker to be used as the back-fed breaker and hook the interlock Tab A into the slot located at the lug end of the branch breaker.
6) Press down against the face of the hold-down bracket to seal it against the breaker.
7) Secure the hold-down bracket to the base with the new interior mounting screw B (Figure 1), provided in the kit and torque to 35 lb-in (4 N-m)

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric Canada

Attachment(s)
PK5RK Instructions.pdf [163.63 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings