Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How does the LK150AN Neutral/Ground lug install into QO or Homeline load center?
Issue:
Product Design Features

Product Line:
QO or Homeline Load Centers

Resolution:
The LK150AN branch neutral/ground lug will install on one of the branch neutral bars of the load center interior or can be installed on a PK__GTA ground bar installed in the load center.
The LK150AN will mount on the top of the bar by removing the appropriate number of wiring binding screws as pointed out in the instructions that come with the kit. The LK150AN will accept (1) #2 - 3/0 Al/Cu AWG wire.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger Label

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center.
3) Remove 3 adjacent wiring binding screws A from the appropriate branch neutral bar.
NOTE: For the 1phase and 3phase QO load centers use the inner neutral bars closest to the Main Breaker or Main lugs on either the right or left side.
4) Installed the neutral lug B as shown in the instructions and tighten the mounting screw C to 50 lb-in (5.6 N-m) using a T-20 Torx driver.
5) Apply the torque label provided in the kit, to the enclosure near where the neutral lug terminal is mounted.
6) Install the appropriate wire size into the neutral lug and see the torque label for the wiring binding screw torque.


NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Label

Schneider Electric Canada

Attachment(s)
LK150AN Instructions.pdf [82.73 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings