How can we help you today?

How can the Door be Reversed on a NSYS3DC Enclosure?

Issue:
Identify how to reverse the door on a NSYS3DC enclosure

Product Line:
Universal Enclosures

Environment:
NSYS3DC Enclosures

Resolution:
The door for the NSYS3DC can be removed as well as the hinges. The enclosure is designed to accept installation of these hinges on either side. Please see attached instructions on the transition.  Since the NSYS3DC is symmetrical, it is also possible to rotate the NSYS3DC enclosure 180 degrees as well as rotate the locking mechanism if no cable glands have been installed.

Schneider Electric Canada

Attachment(s)
ENNA07900-T.pdf [1.15 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors