Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
For part number HMISCU6A5 are the digital outputs relay outputs or transistor outputs
Issue:
Are the Discrete outputs on the HMISCU6A5 relay or transistor?

Environment:
Applies to HMISCU6A5 and HMISCU8A5

Resolution:
The rear module is equipped with 8 relay and 2 transistor outputs. The transistor outputs are fast outputs FQ0 and FQ1

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings