Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement cam part numbers for the 9001KXS selector switches?
Issue:
9001KXS selector switch cam replacements

Product Line:
Push Buttons and Operator Interface

Environment:
9001 type KX

Cause:
Replacement parts

Resolution:
The replacement cams are the same as those for the 9001KS and 9001SKS selector switches:
Class 9001
CamType
BK13B
CK13C
DK13D
EK13E
FK13F
GK13G
HK13H
JK13J
LK13L
M3105402402

See attached instruction bulletin to identify the cam type of your selector switch.

Schneider Electric Canada

Attachment(s)
65013-009-08_01.pdf [1.7 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings