Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Correct Part Number for LA9D115603/604
Issue:
What is the correct part number for a LA9D115603/604?

Product Line:
Digest 177 Section 18:  Contactors and Starters IEC

Environment:
North American Products

Resolution:
There are two parts marked LA9D115603/604, selection should be made based on the contactor in use:
The LA9D115603 is the connector piece supplied with the LC1D115 and LC1D150 three pole contactors.
The LA9D115604 is the connector piece supplied with the LC1D115004 four pole contactor.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings