Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the default settings for the serial communication port on a LINK 150?

Issue:
User would like to know what the default settings are for the serial port on a Link150 Gateway.

Product Line:
Link150 (EGX150)

Environment:
Ethernet Gateways

Cause:
User may want to configure his daisy chain of devices to match that of the default settings for the Link150

Resolution:

See table below  for Serial Port Settings

Description

Settings

Mode

Master

Physical Interface

RS-485 2-Wire

Transmission Mode

Automatic

Baud Rate

19200 bps

Parity

Even

Stop bits

Auto

Termination

Enabled

Biasing

Enabled

Response Timeout

3 seconds

Remote Device Connections

Feature used only for Link150 in slave Mode

Port

502


Documentation: EcoStruxure Link 150

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings