Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TeSys T Average Current Register

Issue:
What register address contains average current?

Product Line:
TeSys T Motor Management Controller

Environment:
TeSysT

Cause:
Programming

Resolution:
The registers for average current (x 0.01 A) are 500-501, it is a UDInt variable type using two bytes which is why you need both registers.

See attached for more information on the communication protocols and variables for the Modbus TCP/EtherNet IP devices

Schneider Electric Canada

Attachment(s)
Ethernet Modbus TCP IP Comm Protocol and Variables.pdf [1.57 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings